Technical FAQs

Ask a Question

How do I use the Scope function of SoMove with Lexium 32 servo drives?

The Scope function within SoMove can be used to aid in tuning of the drive as well as capturing parameters while the drive is operational to aid in cofiguring the drive and or the PLC controlling the dirve for optimal performance.

There is an attached PDF file you can use to learn the basics of using the Scope as well as a video to provide further understanding of using the scope.

 
Was this helpful?
What can we do to improve the information ?