Technical FAQs

Ask a Question

What can trigger an 061 fault on SR3B261FU Zelio logic relay?

Issue:
Relay stopped working and shows 061 under the fault. 

Product line:
Sr3 Zeliologic Smart Relay

Environment:
SR3 expandable units

Cause:
Extension module programming or connection

Resolution:
This can be triggered at the beginning of RUN on the smart relay application and the program is incompatible with the Input/Output extension physically connected to the power supply.
You have to retreive the program in order to know if the expansion is correctly defined in the program.

Some possible reasons for the error
Expansion physically connected but not defined in the program
Expansion not present but defined in the program
A wrong expansion module is connected
Expansion module is defective.
Was this helpful?
What can we do to improve the information ?