Technical FAQs

Ask a Question

What is the part number for the power connector of the XBTGT7340?

Issue:
Need a replacement power connector for Magelis XBTGT

Product Line:
XBTGT5330, XBTGT5340, XBTGK5330, XBTGT6330, XBTGT6340, XBTGT7340

Resolution:
The replacement part number for the power connector of the XBTGT5/6/7 range is XBTZGPWS2. The product is a pack of 5 connectors.

The Phoenix Contact part number for the Schneider Electric part is: 1848009 (GMVSTBW 2.5-7.62)
 
Was this helpful?
What can we do to improve the information ?