Browse FAQs

How to create a slideshow of dashboards/other components in EcoStruxure Building Operation 3.0 Webstation.

Published date: 31 July 2019

Follow below steps to create a slideshow in WebStation:
  • In WebStation, right-click the folder where you want to create the slideshow.
  • Click Create Slideshow .
  • In the Create object - slideshow dialog, in the Name box type a name for the slideshow and Click OK .
  • Click Configure .
  • In the Speed(s) row, enter the interval between dashboards.
  • Click Add.
  • In the Select - Initial path dialog box, select a dashboard and Click OK .
  • Repeat step 7 to 9 to add more dashboards to the slideshow and Click OK.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.