Technical FAQs

Ask a Question

M series programming cable pinout

The shared single DE9 interface can be split by using the Serial/System Port Adaptor. This adaptor is provided
with each digital mode M-Series. The adaptor is a DB9 (Male) to DB9 (Female) and RJ45 socket. This provides a
connection for user data (User Data port) and configuration/diagnostics (System Port).


M series programming cable pinout DB9(PC) to RJ45 (connects to M series adapter)


 
Was this helpful?
What can we do to improve the information ?