Technical FAQs

Ask a Question

Does Vamp 255 supports Ethernet IP & Modbus TCP communication at same time

Yes, Vamp 255 supports Ethernet IP & Modbus TCP communication at the same time. User needs to enable both the protocols in Protocol configuration.
Make sure the port number for Ethernet Ip is 44818 & port number for Modbus TCP is 502.

Use "simple tester tool" to fetch the data. You can find the tool in the below-mentioned link 
https://m.vamp.fi/documentation/ 
Was this helpful?
What can we do to improve the information ?