Technical FAQs

Ask a Question

What are the address details of Time Synchronization over IEC-103 protocol in MiCOM P225/P220

On P225/220 time synchronization over IEC 103, Please use below address to write the time from your master. Date format setting (IEC / Private) will not affect time synchronization over IEC 103.

ASDU TYPE 6
COT 8 
FUN 255
INF 0 

Refer the atatcment for Address details & traces 
Was this helpful?
What can we do to improve the information ?