Technical FAQs

Ask a Question

Does Micom P127 follow IEC EI Curve

Please refer the extract from the User manual of MiCOM P12y, the same curve will be applicable for P12x also as Curve representation is not available in p12x manual 

The equation is valid for 1.1 ≤ I/Is ≤ 20. 

 
Was this helpful?
What can we do to improve the information ?