Browse FAQs

How to Configure AS-B or AS-P Server as a DHCP Server in EBO.

Published date: 31 July 2019

To configure SmartX AS-B or AS-P server as a DHCP Server, follow the below steps:-

1. In Device Administrator, click Servers and then select the SmartX AS-B or AS-P server you want to use as a DHCP server.
2. Click Ethernet 2 Configuration.
3. In the Ethernet 2 mode list, select Dual IP.
4. In the DHCP mode list, select Server.
5. Click Apply.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.