Browse FAQs

Why EcoStruxure BMS Server Failed to Create Backup Set.

Published date: 31 July 2019

Kindly follow below mentioned each step until issue get resolved:-

1. Ensure that a backup is not already in progress.
2. Ensure that the backup set size does not exceed the single SmartX server backup partition disk space.   If the disk space is exceeded, the probable cause can be an exceeded amount of trend logs.
3. Check for an error in one of the modules participating in the backup, or in the backup module itself.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.