Browse FAQs

While installing the Report Server (EBO/SBO), the installation stucks at the message saying 'Database already exists'.

Published date: 01 August 2019

The EBO/SBO Report Server installation stucks while proceeding with creation of new database, it indicates that a RS database is already present at the below location. 
C:\Program Files (x86)\Schneider Electric EcoStruxure\Building Operation WebReports\Database Files

It shows that an earlier/higher/same version is already installed so you need to delete the existing database (if earlier data is not required) first or you can select upgrade existing database (if earlier data is required)
as per the requirement.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.