Browse FAQs

Recommendation for connecting LTMR controller and the LTME expansion module

Published date: 31 July 2019

It is recommended to mount the LTMR controller and its LTME expansion module side by side with the, LTME expansion module on the left side of the LTMR controller and connected by the LTMCC004
connecting jumper (1).

If it is not possible to mount the LTMR controller and its LTME expansion module side by side:
 Use only the shielded cables LTM9CEXP03 (2) or LTM9CEXP10 (3) cables to connect them.
 Ground the shielded cable.
 Separate the LTM9CEXP•• connection cables from all other power or control cables to avoid EMC
disturbance.

For more clarification kindly check attached snapshot

Was this helpful?

What can we do to improve the information ?