Browse FAQs

How to set speed around reference in ATV320 from HMI local display

Published date: 31 July 2019

Basic parameters for speed around reference:-

Set Fr1 – LCC (HMI)
Set Full àCtl- à CHCF à SEP (Because control command is from terminal and frequency reference is from local HMI)
Set Full à Fun- à SrE à uSi à LIx
Set Full à Fun- à SrE à dSi à LIx
Set à Fun- à SrE à SrPà % (Reference Speed i.e Fr1)

Note - If Fr1 is set to 50 Hz and SrP is set to 50%, then the speed will only go up to 50% of 50, i.e. 25Hz.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.