Browse FAQs

What is the meaning of ‘Max Event Stored’ error in Unity Pro or Control Expert. How to resolve it.

Published date: 31 July 2019

This value (between 0 and 32000) defines the maximum number of time stamping events that can be stored in the PLC global event buffer. 
See the PLC → Memory Consumption... to know the memory size used and refine this value if needed. 
When building the project, if this value is too small a message gives the exact value to select. Set the exact value and then the issue will be resolved.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.