Browse FAQs

How to check if ATV310 drive is in local or remote.

Published date: 31 July 2019

There are three LED lights on the left side of the drive HMI screen.

When all three LED's are blinking simultaneously, then the drive is in 'Local Mode' otherwise it is in 'Remote Mode'

ATV310 can be converted from Local to Remote or Remote to Local by simply pressing the 'Mode' button for 3 seconds. 



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.