Browse FAQs

What is the best practice for grounding multiple ATV drives.

Published date: 31 July 2019

For correct grounding procedure make sure of the below points:

-- Ground resistance must be below one ohm.
-- When grounding multiple drives you must connect each one separately
-- Do not loop ground cable or connect them in series.

Check the below attachment for reference.

Was this helpful?

What can we do to improve the information ?