Browse FAQs

What is the maximum number of BMENOP0300 modules that can be mounted on a local rack.

Published date: 31 July 2019

The maximum number of BMENOP0300 modules that can be mounted on a local rack is determined by your choice of CPU. The maximum numbers of communication modules, including BMENOP0300 modules, supported by M580 CPUs are as follows:

BMEP581020  = 2
BME•5820•0  = 2
BMEP5830•0  = 3
BME•5840•0  = 4
BMEP585040  = 4
BME•586040  = 4

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.