Browse FAQs

What is the maximum number of simultaneous client connections possible with BMENOP0300.

Published date: 31 July 2019

The maximum number of simultaneous client connections possible with BMENOP0300 is 16 connections.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.