Browse FAQs

Can we use BMXCRA31200 adapter to connect safety I/O modules to the M580 safety PAC.

Published date: 31 July 2019

A BMXCRA31200 adapter cannot be used to connect safety I/O modules to the M580 safety PAC.

Communications between the safety PAC and safety I/O modules installed in an RIO drop are made through an adapter module installed on the RIO drop, either:
  •  a BMECRA31210 adapter, for an Ethernet rack, or
  •  a BMXCRA31210 adapter, for an X Bus rack.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.