Browse FAQs

Can we use BMXNRP0200 or BMXNRP0201 fiber optic repeater modules with M580 Safety system.

Published date: 31 July 2019

Yes, we can use BMXNRP0200 or BMXNRP0201 fiber optic repeater modules with M580 Safety system to extend the physical link between the CPU and Copro in the local rack and the adapter in the RIO drop.
Fiber optic repeater modules enhance RIO network noise immunity and increase cabling distance while maintaining the full dynamic range of the network and the safety integrity level.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.