Browse FAQs

How BMXERT1604T is different from the regular discrete input modules

Published date: 31 July 2019

The BMXERT1604T module features all the characteristics of a regular 16-channel discrete input module. In addition, the BMXERT1604T module has a time stamping function which records the change (rising or falling edge) of each input channel. To ensure the precision of time stamps, the module is able to receive time codes from a GPS or DCF77 receiver. 
The 16-channels discrete input can also be used as counter inputs; the counters feature increasing counting with the clear function. 
The BMXERT1604T module inputs are compatible with the following rated voltages: 24 Vdc, 48 Vdc, 60 Vdc, 110 Vdc, and 125 Vdc. The inputs use positive (sink) logic.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.