Browse FAQs

What are the functions supported by BMXERT1604T

Published date: 31 July 2019

The BMXERT1604T module has16 descrete inputs that can be configured with the following 3 main functions:
Counter: This function counts pulses from the discrete input channels.
Discrete input: Standard discrete input without time stamping.
Time stamping: The discrete input with the time stamps recorded to mark input state changes.

The inputs are in 4 groups that contain 4 input channels in each group. Input functions can be configured by input group:
Input Group Input Channels Selectable Functions
0 0, 1, 2, and 3 Only time stamping
1 4, 5, 6, and 7 Counter
Discrete input
Time stamping (default)
2 8, 9, 10, and 11 Counter
Discrete input
Time stamping (default)
3 12, 13, 14, and 15 Counter
Discrete input
Time stamping (default)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.