Browse FAQs

Can I take the backup of the security system configuration in Vijeo XL

Published date: 31 July 2019

You can back up your project's security system configuration by exporting it to a file. You can also import a configuration either from a file or from another runtime project.

To export the security system configuration:

  1. In the main Security System dialog, click Backup. The Import/Export dialog is displayed.
  2. Click Export to file. A standard Save As dialog is displayed.
  3. Specify a file name and location for the file, and then click OK.

The exported file is encrypted, using the main password configured in the Security System dialog.

Tip: You can also export the configuration during runtime by calling the ExportSeruritySystem function.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.