Browse FAQs

How can I import security system configuration from other project in Vijeo XL

Published date: 31 July 2019

If your project's security mode is set to Distributed – Server, then you can import a configuration from another project if:

  • The other project's security mode is set to Distributed – Client, and its server settings are configured to use your project as the server; and
  • The other project is currently running on the same network.
To import the security system configuration:
  1. In the main Security System dialog, click Backup. The Import/Export dialog is displayed.
  2. Click Import from client station. The Import Security from Client Station dialog is displayed.

    The dialog shows a list of runtime projects that are using your project as their security system server. Each project/client listing includes a time stamp that shows when it last cached the security system configuration.

  3. Select a client station, and then click Import from client. You will be prompted for the configuration's main password.
  4. Type the password, and then click OK.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.