Browse FAQs

How can we make screens, symbols, and worksheets password protected in Vijeo XL

Published date: 31 July 2019

Screens, symbols, and worksheets in the Project Explorer can be password-protected. You can assign individual passwords to each file, or you can assign a single password to all files in the project

Assigning a password to a single file:

To assign a password to a single project file:
  1. In the Project Explorer, find and right-click the desired file, and then click Password Protection on the shortcut menu. The Edit Protection dialog is displayed.
  2. Type the new password, and then type it again to confirm.
  3. Click OK to close the dialog.

The file is now protected. The next time you try to open it, you will be prompted for the password.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.