Browse FAQs

How can we set Auto Log Off after a certain period of inactivity in Vijeo XL

Published date: 31 July 2019

  • Open the Security System dialog, and then click Groups; or
  • Then click on Advanced button
  • Group Account Advanced window will open (as shown below), select the Auto LogOff tab:


Set the Log Off after time in minutes
It means the number of minutes after which the current user must be logged off automatically. If this field is left in blank (or with the value 0), the current user is never logged off automatically.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.