Browse FAQs

How can we clear password from the screens, symbols, and worksheets in Vijeo XL

Published date: 31 July 2019

Screens, symbols, and worksheets in the Project Explorer can be password-protected. You can assign individual passwords to each file, or you can assign a single password to all files in the project

To clear a password from a single project file:

  1. In the Project Explorer, find and double-click the desired file to open it. You will be prompted for the password.
  2. With the file open for editing, right-click the file in the Project Explorer and then click Password Protection on the shortcut menu. The Edit Protection dialog is displayed.
  3. Leave the New password and Confirm password boxes empty.
  4. Click OK to close the dialog.

The file is no longer protected. You can open the file without being prompted for the password.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.