Browse FAQs

What changes have been introduced for the secondary ethernet port of AS-P/AS-B from EcoStruxure Building Operation 2.0 onwards.

Published date: 01 August 2019

The Device Administrator has expanded the possibilities to configure the secondary Ethernet port. It can now be configured as a separate network. The new secondary network can be
configured the same way as Ethernet 1 with both static IP address and as a DHCP client. A new feature for this network is that it can also be configured to act as a DHCP server. The intention
is to use the feature to host a private network with IP connected sub devices. The IP range of this network will be 10.110.210.X where the AS-P/AS-B always can be found on 10.110.210.1.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.