Browse FAQs

While opening wireshark for network analysis, it shows a warning 'No interfaces found', NPF driver is not running etc. and no network interfaces can be seen.

Published date: 01 August 2019

This is because the NPF driver is not running. Close wireshark and follow below steps:
-Open command prompt and 'Run as Administrator'.
-Type 'net start npf' (without inverted commas) and hit enter
-You should see the message that NPF driver has been started successfully.
-Now wireshark should run and show the list of interfaces.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.