Browse FAQs

Can the Altistart 48 use Fast acting fuses on the line power?

Published date: 06 August 2019

Issue:
Fact acting fuses protecting the ATS48

Product line:
Altistart 48 softstart controller

Environment:
all

Cause:
Documentation does not show fact acting

Resolution:
Fast acting fuses are not recommended.  The starting currents on a softstart can be upwards of 400% or more for several seconds.  It would be recommended to use time delay fuses only.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.