Browse FAQs

What are the part numbers for replacement gaskets for the Magelis HMIGTU panels?

Published date: 09 August 2019

Issue
I need to perform regular maintenance to ensure that the NEMA4X or IP66 rating on my HMI and cabinet are maintained. What are the replacement gaskets for the Magelis HMIGTU panels?
 
Product Line
Magelis HMIGTU
 
Environment
Physical HMI
 
Resolution
The part numbers for the replacement gaskets that the HMIGTU supports are as follows:
HMIZD53W…………..for HMIDT351 (7" Wide)
HMIZD55W…………..for HMIDT551 (10" Wide)
HMIZD56W…………..for HMIDT651 (12" Wide)
HMIZD55………………for HMIDT542 (10.4")
HMIZD56………………for HMIDT642 (12.1")
HMIZD57………………for HMIDT732 (15")
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.