Browse FAQs

Power Monitoring Expert v8.x & 9.0 –EM6436 dual source meter consume S type license instead E type.

Published date: 13 August 2019

 Issue
In PME v8.x and 9.0 when EM6436 dual source meter is added in MC, it consumes High-End device license instead of Entry Range device license.

Environment
PME Licensing

Cause
This appears to be a bug in PME v8.x and PME 9.0.

Resolution
Run attached hotfix (exe) file where PME is installed.

Note: In case of distributed architecture, run exe in Application Server.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.