Browse FAQs

PSO9.0 MicrologicX (MTZ) driver crashing the IO Server in absence of Default Gateway information and Ethernet cable removed from eIFE (R6025)

Published date: 14 August 2019

Issue:
IO Server crashed in PSO9.0 while communicating using MicrologicX(MTZ)

driver in following condition.

Default Gateway in IFE: Set to 0.0.0.0
 
  • Network cable removed from eIFE
  • IO Server crash in PSO every time

 
  • PSO 9.0 CU#2
  • PowerLogic Driver version is 4.3.6.1
Runtime Error!
R6025 – Pure virtual function call

Resolution:
Set Default Gateway in eIFE. If there is no Gateway information, set xxx.xxx.xxx.1 based on eIFE IP address.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.