Browse FAQs

What does ``direct acting`` mean for the 9001KA contact blocks?

Published date: 04 June 2019

Issue:
9001KA operation

Product Line:
9001 Type K and SK, 30mm Push Buttons

Environment:
n/a

Resolution:
Direct acting means that the contact block operates at the same speed as the button is pushed or selector switch is turned.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.