Technical FAQs

Ask a Question

What is the difference between D3 and D voltage code for the low consumption D-Line contactors?

Issue:
Low consumption D-Line contactors

Product Line:
Contactors and Overload Relays

Environment:
TeSys™ D Contactors and Overload Relays

Resolution:
Both coils are rated the same DC voltage.  D3 incidcates the coil provides integral transient suppression.
Was this helpful?
What can we do to improve the information ?