Browse FAQs

PME 7.2.2 web application HTTP Error 500.21 - Internal Server Error Handler "PageHandlerFactory-Integrated" has a bad module "ManagedPipelineHandler" in its module list

Published date: 15 March 2019

Issue
Attempting to access the PME 7.2.2 Web application in a browser yields the following error:
[Error Summary]
HTTP Error 500.21 - Internal Server Error
Handler "PageHandlerFactory-Integrated" has a bad module "ManagedPipelineHandler" in its module list

Environment
PME 7.2.2 Web Applications

Cause
.NET was not registered with IIS during the upgrade or re-install.

Resolution
Run the following command in the Windows command line or powershell as administrator to re-install .NET.
%windir%\Microsoft.NET\Framework\v4.0.30319\aspnet_regiis.exe -i


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.