Technical FAQs

Ask a Question

Filter results

Clear
Can you use an external 24VDC source to control an ATS48 softstart?
Issue: Can you use an external 24VDC source to control an ATS48 softstart?  Product Line: Altistart 48, ATS48 Environment: All Cause: N/A Resolution:...
Where can I find basic programming information for ATV drive?
Issue: Basic programming information for ATV drive? Product Line: ATV930 Environment: All Cause: Basic programming. Resolution: Under drive menu:...
ATV630 and it did not come with an instruction manual.
Issue: What is the part number for the ATV630 programming manual? Product Line: ATV630, ATV650, ATV660 Environment: All Cause: Manual did not come...
Can the ATV630 be programmed to run two pumps and alternate them based on run time?
Issue: Need to program the  ATV630 to run two pumps and alternate them based on run time Product Line: Altivar 630 Environment: All Cause: Has two...
How do you set up an Automatic Restart on the ATV312 drives?
Issue: How do you set up an Automatic Restart on the ATV312 drives? Product Line: Altivar 31 and 312 Environment: All Cause: Wants the drive to do...
How can I setup a permanent magnet synchronous motor on an Altivar Process Drive?
Issue: Setup a permanent magnet synchronous motor on an Altivar Process Drive? Product Line: Altivar Process Drive (ATV630, ATV930, ATV650, ATV950,...
Can you run a smaller test motor on a ATV630 and ATV930 drive?
Issue: Can you run a smaller test motor on a ATV630 and ATV930 drive? Product Line: ATV630 and ATV930 Environment: All  Cause: Set up drive for test...
Where can I get the SCCR for the ATV71 drives?
Issue: Getting SCCR on the ATV71 drives Product Line: ATV71 Environment: All products of ATV71 Cause: N/A Resolution: Reference the attached Annex...
What is the maximum number of drives you can daisy chain using Modbus TCP/IP on an ATV32
Issue: Maximum number of drives to daisy chain Product Line: ATV32, ATV61 and ATV71 Environment: Modbus TCP/IP Daisy chain part number ATV32 - VW3A3616...
What would cause the ATV320 drives display to flash?
Issue: What would cause the ATV320 display to flash? Product Line:  ATV320 Environment:  All  Cause:  Drive display blinks off and on.  Motor does...
Results 1 - 10 of 100