Technical FAQs

Ask a Question

How do I setup Anti-Jam function on the Altivar 6xx Process Drive?
Issue: How do I setup Anti-Jam function on the Altivar 6xx Process Drive? Product Line: Altivar 6xx Environment: All serial numbers for Altivar 6xx ...
Are lugs included with ATS22 Soft Starts?
Issue: Are lugs included with ATS22 Soft Starts? Product Line: ATS22 Environment: All Cause: N/A Resolution: Smaller units (ATS22D17 thru ATS22D88)...
What is the Pin-out for TSXCAP030 cable.
TSXCAP030 is a pre fabricated cable with 25pin Sub D connector. It is a straight cable with pin to pin connection. Go through the attached drawing...
Do we have any product reference for the female screw connector used in BMXEIA0100.
we can use product reference # 1841909 from Phoenix contact.  Refer the attached Datasheet for your ready reference. 
What are the necessary tools required to crimp MA0329001 F connector and RG-6 cable.
Below are necessary tools required to crimp MA0329001 F connector and RG-6 cable:  Coaxial Cable Cutter : 600558000  Coaxial Cable stripper : 490RIO00400 ...
Which are the materials used in Compact NSX connection terminals.
The material used in the Compact NSX terminal connectors is as below:   Compact NSX100-250 : Copper (Cu) + Tin coating   Compact NSX 400-630: Copper...
What is the Pin-out for quantum expander module 140XBE10000 cable 140XCA71703.
The Pin-out for expander module 140XBE10000 cable 140XCA71703 is attached herewith.  
Where can one download the embedded ethernet manual for ATV630 process drive?
Issue: Where can one download the embedded ethernet manual for ATV630 process drive? Product Line: Altivar 600 Process Environment: All serial numbers...
What is the part number for the Ethernet IP / Modbus TCP IP option card for the ATV32 series drives?
Issue: What is the part number for the Ethernet IP/Modbus TCP/IP option card for the ATV32 series drives? Product Line: Altivar 32 series drives....
Where can I find the heat dissipation for the ATS48 Softstarters?
Issue: Heat dissipation for the ATS48 Softstarters? Product Line: ATS48 Environment: All products of ATS48 Cause: N/A Resolution: Reference the table...
Results 1 - 10 of 100