Technical FAQs

Ask a Question

Filter results

Clear
Where can I find the heat dissipation for the ATS48 Softstarters?
Issue: Heat dissipation for the ATS48 Softstarters? Product Line: ATS48 Environment: All products of ATS48 Cause: N/A Resolution: Reference the table...
How can I perform a competitive cross reference to an Altivar Drive or Altistart Softstart?
Issue: Customer would like to cross reference a non-Schneider drive or softstart to one of our products (Altivar or Altistart). Product Line: All...
Is the ATV630 (or ATV930) Process drive available with 1 phase input and 3 phase output?
Issue: Is the ATV630 (or ATV930) Process drive available with single phase input and 3 phase output? Product Line: Altivar 630 Altivar 930 Environment:...
Is the S-Flex drive available in Nema 3R outdoor enclosure?
Issue: Is the S-Flex drive available in Nema 3R outdoor enclosure?   Product Line:  S-Flex   Environment:   3R enclosure Cause:   n/a Resolution: ...
Is the Canalis range of products KBA, KBB, KDP halogen free.
Yes, the Canalis range of products KBA, KBB and KDP are halogen free. The Declaration of Conformity is attached.
Are conduit kits available for the Altivar Process Drives?
Issue: What are the conduit kits for the Altivar Process Drives? Product Line: Altivar Process Drive (ATV630, ATV930) Environment: All serial numbers...
What are the Environmental characteristics of Enerlin'X IFE Ethernet Interface for LV Circuit Breaker.
Please refer below table for the Environmental characteristics of Enerlin'X IFE Ethernet Interface for LV Circuit Breaker.
What is the storage temperature of STI isolatable fuse-carriers.
The storage temperature of STI isolatable fuse-carriers is -40°C to +80°C.
What are the part numbers for the remote keypad and mounting accessories for Altivar Process Drives?
Issue: What are the part numbers for the remote keypad and mounting accessories for Altivar Process Drives? Product Line: Altivar Process Drives Environment:...
How can I prevent Undervoltage faults on ATV61 drives?
Issue: How can I prevent Undervoltage faults on ATV61 drives? Product line: ATV61, Altivar 61, ATV71, Altivar 71 Environment: All Cause: Temporary...
Results 1 - 10 of 62