Technical FAQs

Ask a Question

Filter results

Clear
Vijeo Designer Project won't build and shows error: Please check you Driver/Device configuration or variable settings
Issue: Vijeo Designer Project won't build and shows error: Please check you Driver/Device configuration or variable settings Product Line: Vijeo Designer...
What are the Share-UPS and Interface Expander modes of operation?
Issue What are the Share-UPS and Interface Expander modes of operation? Product Line   UPS Device Management AP9607/AP9607CB Interface Expander SmartSlot...
Getting message "FBDCG(-806)" in concept Software during online modification(Download changes).
Explaination of message is below: FBD CG : Function Block Diagram Code Generation  -806   : Call to object database failed ,Problems with database...
Why do I get the Error "Application has halted due to: Unhandled, java/lang/NullPointerException IVM: except.c: line 322" on a Magelis HMI?
Issue Why do I get the Error "Application has halted due to: Unhandled, java/lang/NullPointerException IVM: except.c: line 322" on a Magelis HMI?...
Getting message "External Power supply is required" in the power supply budget of BMXCPS3020.
The M340 DC power supplies do not supply any 24 VDC for External field devices or BMXCPS2010 or 3020 power supply has no inbuilt sensor DC supply...
SoMachine V3.1 gives build error '3S CANopenStack 3.4.1.70: Outdated library version...' Why. How to solve this build error.
In case user imports a SoMachine V3.1 project archive, which may contain the original version 3.4.1.70 of the CANopenStack library, the new one will...
In SoMachine whenever I download the application into Simulator it creates Program Exception while the same application is running in PLC without any problem. What could be the reason behind it.
The reason behind if the application program has task watchdog enabled and when it is being used with Simulator it creates program exception. It is...
Getting Message "OLN-11575" in concept V2.6 SR7 while connecting to Controller over Modbus Plus.
Causes:  1. This error comes if you have not set the correct interrupt in the modicon.ini file for modbus plus. 2. Modbus plus card is not available...
When I am using Web Client to access Vijeo Citect pages, I am getting the error as "Software Protection Failure / Key not found" and do not get any data on the graphic pages.
There can be more than one cause for this error on a web client machine. Here are few known issue that may cause this problem: 1. License Availability:...
LXM32M driver stops with E7344 error. What are the different cause of this error and how to resolve it.
Error E7344 occur because hyperface provides the drive with sine cosine signal and incremental position. The drive compares both and when there`s...
Results 1 - 10 of 100