Technical FAQs

Ask a Question

Filter results

Clear
What are the Share-UPS and Interface Expander modes of operation?
Issue What are the Share-UPS and Interface Expander modes of operation? Product Line   UPS Device Management AP9607/AP9607CB Interface Expander SmartSlot...
How do you update the M241 or M251 firmware using SoMachine Controller Assistant?
Issue How do you update the M241 or M251 firmware using SoMachine Controller Assistant? Product Line Modicon M241 PLC Modicon M251 PLC EcoStruxure...
Which communication protocol is used between a Compact NSX and display FDM121.
The communication protocol used between the Compact NSX and FDM121 display is Universal Logic Plug (ULP). This a Schneider Electric internal protocol.
Where to download M580 Firmware?
Issue: Where to download M580 Firmware? Product Line: M580 Resolution: The M580 Firmware can be downloaded from here: https://www.schneider-electric.ca/en/download/range/62098-Modicon%20M580%20High-end%20Controller/?docTypeGroup=88181372-Software%2FFirmware...
Is it possible to update the firmware of the Altistart 48 control board (VX4G481).
The best way is to order and replace the new control board with the latest version. It is not possible to update the firmware of Altistart 48 because...
Why does my USB drive show up as a Modicon PLC in the Device Manager?
 Issue: USB drive does not work properly and shows up as a Modicon PLC in the Device Manager of the PC.   Product Line: Modicon PLC   Environment:...
How to install the USB driver for Zelio Soft2 and install USB cable SR2USB01.
Follow the step by step procedure in order to install the USB driver for Zelio Soft2 and the USB cable SR2USB01 for two different operating systems...
How we can communicate Power Logic SCADA ( PLS ) with Allen Bradley MicroLogix 1100 PLC having a TCPIP Port.
You can use the ABMLXEIP driver in Power Logic SCADA for communicating Allen Bradley MicroLogix 1100 PLC , this ABMLXEIP driver will not be available...
On a Magelis XBTGT display unit equipped with a USB port, how can I install a Runtime version that is earlier than the Vijeo Designer
Symptom: In Vijeo Designer, if you try to load an earlier Runtime version onto an XBTGT, the following message is displayed: "You are trying to transfer...
What are the part number and driver for the serial port (9-Pin D-Shell) to USB converter for Modicon Quantum PLC.
The part no. of the Schneider USB to RS232 Converter is TSXCUSB232 Refer the attachment for the TSXUSB232 documentation.   Use the standard Schneider...
Results 1 - 10 of 89