Technical FAQs

Ask a Question

Filter results

Clear
Is it possible to use TeSys GV2 and TeSys GV3 Range MPCB in DC applications?
The TeSys GV2 and TeSys GV3 range MPCB can be used in DC applications as per their technical specifications. Refer the below wiring connection for...
What is the function of battery used in Micrologic Trip unit.
The battery inside the Micrologic keeps the Clock and Calendar maintained when the Control Supply has failed. This battery also allows the testing...
How do we know that Catridge is damaged in Surge Protection device.
On the cartridge itself there is a color indication regarding its life, if its white in color it means it in operation and if it is red in color its...
What is the new tag point count licensing in Citect SCADA V7.0 ?
In CitectSCADA 6.10 or earlier, multiple tags that share the same I/O device address will be counted as a single I/O point. This is calculated at...
Is it possible to use Altivar 71 Drive for control of the Synchronous Motor.
Yes, Altivar 71 Drive can be used for control of the Synchronous Motor.  Note:   1. The Drive should be programmed for Open-Loop Control.   2. De-rate...
How to connect XPSMC via USB, using TSXCUSB485 USB converter?
XPSMC + TSXCUSB485 hardware connection XPSMC + TSXCUSB485 software rules
What is the maximum motor cable length allowed between the Sinus Filter and Altivar 71 Drive.
The maximum motor cable length allowed between the Sinus Filter and Altivar 71 Drive is 1000 Meters.
I would like to know that OFS v3.40 will be supported on Windows 7 , 64 bit system or not. 
OFS v3.40 will supports Windows 7 , 64 bit system but some of the drivers like Ethway, ISAway & FIP FPC10 were not supported on Windows 7 64 bit.  
What is the accuracy of the Premium PLC CPU real time clock.
Real time clock accuracy: Accuracy of the real time clock is one second (%SW50) +/- 200ms. Resolution of the real time clock is one second (%SW50)...
Which are the latest GSD file revisions for ProfibusDP communication board of the Altivar 71 Drive.
The latest GSD File revisions required for ProfibusDP communication board of the Altivar 71 Drive are as follows:  1. The correct revision of GSD...
Results 1 - 10 of 93