Technical FAQs

Ask a Question

Is the braking transistor inbuilt in Altivar 71 Drives?
The Braking transistor is inbuilt in maximum ratings of Altivar 71 Drive. The following Altivar 71 Drive ranges ATV71HpppM3, ATV71HpppM3X, ATV71H075N4…HC16N4,...
What are the Share-UPS and Interface Expander modes of operation?
Issue What are the Share-UPS and Interface Expander modes of operation? Product Line   UPS Device Management AP9607/AP9607CB Interface Expander SmartSlot...
What is the Pin-out for TSXCAP030 cable.
TSXCAP030 is a pre fabricated cable with 25pin Sub D connector. It is a straight cable with pin to pin connection. Go through the attached drawing...
Do we have any product reference for the female screw connector used in BMXEIA0100.
we can use product reference # 1841909 from Phoenix contact.  Refer the attached Datasheet for your ready reference. 
Is it possible to use Altivar 71 drive with synchronous motor and encoder feedback signal of type SinCos 1 Vpp.
Yes, it is possible to provide speed feedback of signal SinCos 1 Vpp to ATV71 drive. For this user must use ATV71H***N4383 drive(V1.7 and higher)...
Will there be any problem if the MX coil (shunt trip) of NS100 to NS630 is continuously kept powered up.
With the newer design technology there will be absolutely no problems if the MX coil (shunt trip coil) of NS100 to NS630 is continuously kept powered...
Why does the display light of Micrologic 6.2 trip unit of Compact NSX not glow even when the load reading is displayed.
Unlike other range of Micrologic the backlighting or display light of Micrologic 6.2 is not self powered by the primary current.   A separate external...
What is the full name of the abbreviation 'STR' trip unit ? .
 The abbreviation 'STR' has a very old origin. The first generations of trip units were called Statimax and 'STR' refers to "Statimax Trip Release".
What are the different use of SD card in Modicon TM221 PLC series.
The Modicon M221 Logic Controller allows the following types of file management with an SD card:  1. Clone management: back up or restore a complete...
Is 490NOR00003 or 490NOR00005 HSBY fiber optic cable is Flame retardant.
yes , HSBY fiber optic cable i.e. 490NOR00003 or 490NOR00005  is Low Smoke Zero Halogen according to HD.624-7 and Flame-retardant according to NFC32...
Results 1 - 10 of 100