Technical FAQs

Ask a Question

Filter results

Clear
How can I perform a competitive cross reference to an Altivar Drive or Altistart Softstart?
Issue: Customer would like to cross reference a non-Schneider drive or softstart to one of our products (Altivar or Altistart). Product Line: All...
Where might I be able to find Modicon products no longer being actively sold?
Issue Customer is looking for product that is off of active sale. Product line Quantum, A120 Compact, Magelis, 800 series, 200 series, 984 controllers...
Can we get N/C contacts for XD4PA12?
No, there are no options for contacts in the XD4PA range, but normally closed contacts can be added to the XD2GA range using ZB2BE102.
Does Schneider Electric sell AC motors?
Issue: Does Schneider Electric sell AC motors?  Product Line: All Environment: All Cause: N/A Resolution: Schneider Electric does not sell any AC...
Which ATV61 / ATV71 drives are frame size 8?
Issue: Which ATV61 / ATV71 drives are frame size 8? Product Line: ATV61 ATV71 Environment: All 460V/480V Cause: Possible alternatives Resolution:...
How to do conversion of servo motor BSH205 to BMH205.
since 2013 the BSH205 is obsolete and can be replaced by BMH205. There is same physical performance of BSH205 and BMH205 but due to different commercial...
What is the correct substitute for Integral 18 & 32.
Since, the Integral 18 & 32 are discontinued now,the nearest correct substitute is Tesys U DOL motor starter. Please note that Tesys U is a customized...
What are the technical details of DK1JC23 and what is the standard cross reference of DK1-JC23 reference
The DK1JC23 was a 3 poles fuses switch disconnector size 1 fuse rated for 315A maximum. Please refer the attached available catalog page for the technical...
What is the technical specification of GV2P10AE11TQ reference.
GV2P10AE11TQ is the same product as GV2P10 + GVAE11. So this reference has same specification as GV2P10 MPCB with GVAE11.    The TQ suffix denotes...
Can a third party photo cell be used with the light sensitive switches?
No, the light sensitive switches are designed to be used with the photo cells supplied with them.
Results 1 - 10 of 58