Technical FAQs

Ask a Question

Filter results

Clear
Masterpact NW drawout modbus communicable breaker is not able to establish communication via. CCM "Chassis" Module.
It is necessary to synchronize BCM and CCM to get the breaker status, if CCM is not synchronize with BCM, it will not respond.   Following steps are...
What is the function of the Compact Flash memory cards and on which Magelis display units can they be used?
CF (Compact Flash) cards are used to store the following types of information: historical data, recipe data, alarm data, project backups.  We can...
Can I convert an XBTL1000 application (XBTF terminal) to Vijeo Designer (XBTGT/GK terminal)?
We have a Services & Projects offer making it easy to migrate XBTL 1000 applications created on XBTF terminals to Vijeo Designer applications for...
Where can I get a copy of the programming manual for the Altivar 630 Process Drives?
Issue: Where can I get a copy of the programming manual for the Altivar 630 Process Drives?   Product Line: ATV630 drives   Environment: Programming...
Does the Energy Reading remain stored for ME range Energy Meters during power failure.
Yes, the Energy Readings remain stored for the ME range meters during power failure as they are stored in the EEPROM. EEPROM is nonvolatile memory...
What is the effect of selecting the M340 PLC configuration parameter 'Initialize %MWi reset on cold start' ?
When checked, those %MW 's with initial values will be loaded. Any %MW not having an initial value will be cleared (initialized) to 0. If unchecked...
Can Concept error '801 - error opening loadable file' be corrected?
Cause:     Concept is unable to locate a loadable in the Concept \DAT folder when doing a compare or download. Resolution:     Make sure the loadable...
How to open an excel file during runtime in Vijeo Citect.
Below cicode function can be used during runtime for opening an Excel file in Vijeo Citect:   Exec("^""+"C:\Program Files\Microsoft Office\Office11\Excel.exe"+"^"...
How can I prevent Undervoltage faults on ATV61 drives?
Issue: Needs to  prevent Undervoltage faults on ATV61 drives. Product line: ATV61, Altivar 61, ATV71, Altivar 71 Environment: All Cause: Temporary...
How to setup a Fault Status on the Altivar Process Drive?
Issue: How to setup a Fault Relay on the Altivar Process Drive? Product Line: Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960,...
Results 1 - 10 of 100