Technical FAQs

Ask a Question

Filter results

Clear
Is it possible to configure the Quantum Hot standby System without the RIO head 140CRP93200/140CRP93100 while using Unity Pro.
The minimum requirement for Hot standby system is to have One power supply, one CPU and RIO head 140CRP93200/140CRP93100. We can configure the Quantum...
How to change the Node name of M258 controller from USB memory stick.
Below are the steps to change the name of M258 controller from USB memory stick.   1) SoMachine Menu Online /USB mass storage include command SetNodename...
Is it possible to establish communication over modbus RS422 with TSX ETG100.
Yes it is possible, As there is no setting for modbus RS422 protocol in TSX ETG100 however following Steps explained in below attached file  will...
How to setup PM820 relay output for under voltage alarm
To set up the own alarms for default KY digital output or even after installing an input/output module (PM8M2222) via display. For example, you may...
Does the Energy Reading remain stored for ME range Energy Meters during power failure.
Yes, the Energy Readings remain stored for the ME range meters during power failure as they are stored in the EEPROM. EEPROM is nonvolatile memory...
What is the Pin out detail for the Modbus programming cable 110 XCA 20 3000?
The pin out details of the Modbus programming cable 110 XCA 20300 is as shown in the attached.  
What are the different scenarios of Ready LED in Compact NSX?
The different scenarios of Ready LED in Compact NSX is as shown in the attached.   Note: Ensure that the trip unit is correctly supplied i.e. primary...
What is the overvoltage fault threshold of Altivar 31.
The over voltage fault threshold of Altivar 31 is as attached.
Can an impulse-type power supply be used for electrical opening and closing order of Compact NS MCCB?
Yes, the impulse-type power supply (time duration > 20 ms and Voltage level above 0.7Un) can be used for electrical opening and closing of Compact...
What is the reference of Type A or Type B thermostat in Prisma Plus switchboard?
Type C thermostat is available in Prisma Plus, the part reference of which is 08998. The Type C thermostat Reference 08998 can be used as Type A or...
Results 1 - 10 of 100