Technical FAQs

Ask a Question

Is it possible to configure the Quantum Hot standby System without the RIO head 140CRP93200/140CRP93100 while using Unity Pro.
The minimum requirement for Hot standby system is to have One power supply, one CPU and RIO head 140CRP93200/140CRP93100. We can configure the Quantum...
What is the difference in the communication cable TWDXCARJXXX and TSXCRJMD25 used for Twido modbus connection on Port1.
Both the cables are  for different purpose.   TWDXCARJXXX cable is being used for the serial modbus communication where DPT signal of pin 5 is being...
Where should I connect the SZ1RV1202 potentiometer (pot) to the ATV variable speed drives?
The potentiometer part number: SZ1RV1202 must be connected to one of the 0...10 V analog inputs on ATVxxxx range variable speed drives: ATV12 (or...
Can the OA1 output of Tesys U be used with multifunction unit to drive a separate motor contactor.
Output OA1 for Tesys U with base contactor (LUB**) is only used to drive the contactor embedded inside the TesysU contactor base LUB.   In order to use...
What are the Technical specifications of ON/OFF indication contacts (OF) of EasyPact SPS circuit breaker.
The Indication contacts indicate the ON or OFF position of the circuit breaker: >  These OF are rotary type changeover contacts which are directly...
What is minimum system considerations for using PRM module in Quantum ERIO architecture.
To communicate PRM in a Quantum QEIO system you need to deploy the 140NOExxxxx module. You may configure the connection of NOE and PRM as below :-...
Is it possible to have same device ID of multiple LTMR with same master controller (PLC)
It is not possible to have same device ID for multiple LTMR device with single Master controller (For Ex. PLC). There will be conflict in exchanging...
Does the Energy Reading remain stored for ME range Energy Meters during power failure.
Yes, the Energy Readings remain stored for the ME range meters during power failure as they are stored in the EEPROM. EEPROM is nonvolatile memory...
What is the Pin out detail for the Modbus programming cable 110 XCA 20 3000?
The pin out details of the Modbus programming cable 110 XCA 20300 is as shown in the attached.  
Can the existing Full Function Test Kit (FFTK) be used for testing the new Compact NSX MCCB?
Compact NSX can be tested with a new dedicated test kit, Maintenance case reference TRV00910. This TRV00910 test kit works in association with the...
Results 1 - 10 of 100