Technical FAQs

Ask a Question

What cause Error message OLI-21702 in concept software and how to solve it.
Possible causes:  1. One or more sections selected for a download changes exceeds the maximum data size.  2. The PLC memory is too fragmented due...
What are the Technical specifications of ON/OFF indication contacts (OF) of EasyPact SPS circuit breaker.
The Indication contacts indicate the ON or OFF position of the circuit breaker: >  These OF are rotary type changeover contacts which are directly...
How to connect a 2-Wire sensor to Zelio Logic SR3B261FU.
Refer to attached file for a document illustrating connection of 2-Wire sensor to a Zelio Logic SR3B261FU. The input impedance to be used is around...
Is it possible to establish communication over modbus RS422 with TSX ETG100.
Yes it is possible, As there is no setting for modbus RS422 protocol in TSX ETG100 however following Steps explained in below attached file  will...
Why I am getting the compatibility error while downloading the application from Unity Pro to PLC .
The error appears due to the compatibility between the firmware version of CPU in Unity application and the firmware version of actual hardware. Select...
Do we have any Schneider CPU that support freeport protocol.
In M340 range of plc  you can use character mode for a protocol independent communication between two devices. Character mode is a point-to-point...
What is the part number for XAPJ1201SPEC0709 enlosure?
XAPJ1201SPEC0709 enclosure part number is XAPJ1201
What is the replacement for ZB5AT8643M330?
ZB5AT8643M330 has been divided into two parts E-Stop ZB5AT8643M + Label ZBY9330 "EMERGENCY STOP" 
What is the Default user name & password for FTP login of M580 PLC?
Default details are:- Login: datastorage Password: datadownload  
Can I convert an XBTL1000 application (XBTF terminal) to Vijeo Designer (XBTGT/GK terminal)?
We have a Services & Projects offer making it easy to migrate XBTL 1000 applications created on XBTF terminals to Vijeo Designer applications for...
Results 11 - 20 of 100