Technical FAQs

Ask a Question

We need to move the tag values from one IODevice to other IODevice, is there any cicode or functions available for this operation.
For writing tags values from one IO Device to another IO device is possible with a simple cicode using a equal sign like as in below cicode :   ******************************************************...
How to calculate standard deviation for a tag value in Vijeo Citect project?
For calculating the Standard Deviation in Citect, there is a inbuilt function is available " TableMath( ) ". You can use this in cicode as shown below:...
Even defining the HomePage with Computer Setup Wizard, it is not working in XP-Style template.
For setting the required home page you need to add following INI parameters :   [Page]HomePage = Welcome   [Navigation]HomePage = Welcome.
The Printer Button of Vijeo Citect in XP_style page is not working?
For using buttons like Printer you need to set the Citect`s INI parameter for the required port where your printer is connected or if you have installed...
What is the default port for Trend and Alarm server for Vijeo Citect version 7.2?
Defaults port for Trend Server is 2085 and for Alarm Server is 2080 for Vijeo Citect version 7.2.
While configuring the IOServer in computer setup wizard , Server and Control client option is not enabled, how to enable this option?
You need to remember that the network address in your project should be similar to the system`s IP address.
How to configure trends tags for storing trend files for a fixed period?
The configuration of the trend file is should be like as described in the below:  You need to put the following Trend Tag Configuration settings for...
Vijeo Citect Express Wizard not working when used with VJC 7.10 SP1.
On PC`s where no serial ports exist, the express wizard would go into a indefinite loop. This issue has been addressed in the latest Service Pack...
When we should select historical mode in tag item property for historian tag configuration?
This Historical Mode is more suitable for RTU or similar devices where SCADA connection with device is not continuous.   For example ,if you want...
What is the part number of remote display terminal for Altistart 22 SoftStarter?
The part number of remote display terminal for Altistart 22 SoftStarter is VW3G22101.
Results 41 - 50 of 100