Technical FAQs

Ask a Question

How to generate warning message for unused variables in Unity pro project.
Follow the below steps to enable warning message for unused variables:   1. Open application backup in unity pro. 2. Go to Tool menu 3. Go to Project...
Which wiring connector can be used with BMXSRA0405 digital relay output module.
The following Schneider Electric 20-point terminal blocks to fit the 20 pin connector on the front of the module:   1. screw clamp terminal block...
How to detect current out of range alarm in BMXSAI0410.
The BMXSAI0410 module detects a cut wire condition and reports it as a current out of range condition at current value less than 3.75 mA or greater...
At what value of input for BMXSAI0410 channels shows current out of range alarm.
The BMXSAI0410 module detects a cut wire condition and reports it as a current out of range condition at current value less than 3.75 mA or greater...
What is the maximum current allowed on a C-Bus network.
The maximum current allowed on a C-Bus network is 2000mA, this can be provided by any combination of available power supplies, either inbuilt to output...
What is the firmware downgrade limitation for BM*CRA312*0 module.
Below are the firmware downward compatibility limitation for BM*CRA312*0 => do not downgrade a BMECRA31210 PV>=5 to an SV< 2.18 => do not downgrade...
What are the Contact Resistance values for the SF2 range MV Circuit Breaker.
The contact resistance values for the SF2 range MV Circuit Breaker are tabulated below :   SF2 SF2 Fixed SF2 in Mcset SF2 in F400 Contact Resistance...
What are the Contact Resistance values for the Evolis 17.5KV Circuit Breaker.
The contact resistance values for the Evolis 17.5KV Circuit Breaker are tabulated below:   Evolis 17.5KV Evolis 145mm Evolis 185mm Evolis 240mm Fixed...
Is the Canalis range of products KBA, KBB, KDP halogen free.
Yes, the Canalis range of products KBA, KBB and KDP are halogen free. The Declaration of Conformity is attached.
What is the reference of Type A or Type B thermostat in Prisma Plus switchboard?
Type C thermostat is available in Prisma Plus, the part reference of which is 08998. The Type C thermostat Reference 08998 can be used as Type A or...
Results 61 - 70 of 100